Push changes that you make to the remote repository
Push changes that you make to a remote repository to back up the project to a location other than your local computer and provide version control for the project. Changes pushed to the remote repository are available to others who work on the project.
When there are changes to push, the message "Local changes are available to push" appears in the status bar and the
icon displays a blue number with the number of commits to push.
Push to remote
IMPORTANT:
When you push changes to the remote repository, the project must be synchronized or you will be prompted to pull from the remote repository and resolve conflicts. When there are changes to pull, the message "Local and remote changes available to push and pull" appears in the status bar and
displays a blue number with the number of commits to pull.
Pull from remote
- From the open project, select.Push to remote
- If you do not have aFactoryTalk Optix Studiouser identity and therefore are not authorized in GitHub to push changes to the remote repository, the message "Open GitAuthHandler.exe? https://github.oplatform.it wants to open this application" appears to open GitHub and create your identity.
- (optional) To always allow GitHub to open the link to authenticate you, selectAlways allow github.platform.it to open links of this type in the associated app.
- SelectOpen GitAuthHandler.exe. Your identity is added and you are authorized to push changes to the remote repository.
- (optional) If version control is enabled for a local project and you are pushing changes from the local project the first time, you can associate the project with a remote repository:
- InConfigure remote location, inRemote location, type the URL of the remote repository.
- SelectOK.
- If changes are not saved and committed previously, inSave and commit, inCommit message, enter a description of the changes, and then selectOK.
The changes are committed to the remote repository.
Provide Feedback