Compare versions of a project
Compare two different versions of a project by selecting two different committed changes in
View history
.- In the open project, select.View history
- InView history, selectin two different commits to compare.TIP: The differences between the commits are highlighted.
- (optional) To toggle the content that appears inView history, select either:
- All. Toggle to show all content in the project.
- Updates. Toggle to show only the differences between the selected commits. This is the default.
Provide Feedback