View history contents
View history
displays all of the changes committed to a local or remote repository for a project. Example content in 
View history
may include:

Item | Description |
---|---|
A | The first letter of the user that committed the change to the repository. |
B | The commit with the description of the change, the date and time of the commit. Select ![]() |
C | Icon indicates which repository contains the commit. ![]() Local history ![]() Remote history |
D | Indicates a change in the commit from the previous version. Expand the object to see the highlighted values that changed in the object. |
E | Select either All to display the entire contents of the project, or Updates to displays only changes to the selected commits. |
Provide Feedback