Develop a temperature change alarm
Develop an alarm that signals when temperature exceeds a set value.
Application example
![](/content/dam/dita/en/factorytalk-optix/1-10/_images/TemperatureChangeAlarm.png/_jcr_content/renditions/original)
NOTE:
Download a sample project:
TemperatureChangeAlarm.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example
![](/content/dam/dita/en/factorytalk-optix/1-10/_images/TemperatureChangeAlarmDesign.png/_jcr_content/renditions/original)
elect
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback