Create a list of motors
Create a list box populated with motor objects.
- InProject view, right-clickMainWindow (type)and select .
- Hover-over the list box, select, and enterMotorListBox.
- InProperties, create a dynamic link betweenModelandFor more information about dynamic links, see Create dynamic links.
Provide Feedback