Create an acceleration gauge and labels

  1. Create the speed gauge:
    1. In
      Project view
      , right-click
      MotorAccelerationPanel
      and select
      New
      Base controls
      Circular gauge
      .
    2. Hover-over the gauge, select
      Edit
      , and enter
      AccelerationGauge
      .
    3. In
      Properties
      , create a dynamic link between
      Value
      and
      Aliases
      {Motor}
      Motor
      Acceleration
      .
      For more information about dynamic links, see Create dynamic links.
  2. Create the speed label:
    1. In
      Project view
      , right-click
      MotorAccelerationPanel
      and select
      New
      Base controls
      Label
      .
    2. Hover-over the label, select
      Edit
      , and enter
      AccelerationLabel
      .
    3. In
      Properties
      , set
      Text
      to
      Acceleration
      .
  3. Create the speed value label:
    1. In
      Project view
      , right-click
      MotorAccelerationPanel
      and select
      New
      Base controls
      Label
      .
    2. Hover-over the label, select
      Edit
      , and enter
      AccelerationValueLabel
      .
    3. In
      Properties
      , create a dynamic link between
      Text
      and
      Aliases
      {Motor}
      Motor
      Acceleration
      .
      For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.