Develop a label with a localized engineering unit
Create a simple interface that displays temperature in a format that is adjusted for a logged in user locale.
Application example - Celsius degrees (it-IT)

Application example - Fahrenheit degrees (en-US)

NOTE:
Download a sample project:
LocalizedEngineeringUnitLabel.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example

elect
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback