Create a linear gauge
Create a gauge that enables you to see and control the current temperature.
- InProject view, right-clickMainWindow (type)and select .
- Configure the gauge:
- InProperty, create a dynamic link betweenValueand .
- Next toWarning zones, select.
- UnderWarningZone1, create a dynamic link betweenFromandFor more information about dynamic links, see Create dynamic links.
- UnderWarningZone1, create a dynamic link betweenToand .For more information about dynamic links, see Create dynamic links.
- UnderWarningZone1, setColorto#fe1414.
Provide Feedback