Create an alarm
Create an exclusive level alarm that warns about exceeded temperature.
- InProject view, right-clickAlarmsand select .
- InProperties, setHigh limitto60.
- SetAuto confirmtoTrue
- SetMessagetoMaximum temperature exceeded
- Create a dynamic link betweenInput variableand .For more information about dynamic links, see Create dynamic links.
Provide Feedback