- Getting started
- Using the software
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Develop a contact form
Develop a contact form that sends emails to a predefined address.
Application example

TIP:
You can download a sample project from:
ContactForm.zipPrerequisites
- To develop the project
- Save the project.
Select
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback