Create a database with sample data types
Create a database with sample data types to populate and export to a
CSV
file.- Create an Embedded database. See Database.
- Hover-over the database, select, and enterStore1.
- Configure the following table columns:Column numberData type1Int162Int323Float4StringFor more information, see Configure a database table.
Provide Feedback