Develop a solution for importing objects
This design-time script creates objects in the project based on the data from a
CSV
file.
TIP:
You can download a sample project from:
ObjectsFromCSV.zipPrerequisites
In the following example, the
CSV
file contains information about alarms and model variables used by these alarms.
variable,var1,boolean variable,var2,uint32 alarm,alarm1,digital,var alarm,alarm2,analog,var2
#1 column | #2 column | #3 column | #4 column |
---|---|---|---|
Indicates whether you need to create a project variable (keyword variable ) or an alarm (keyword alarm ). | Indicates the name of the node to be created. | Indicates the datatype to use to create the variable:
| Indicates the variable to point the alarm to. |
TIP:
The
CSV
file is a part of the sample project. You can also download the CSV
file individually from: alarms.csv- To develop the project
- Save the project.
Provide Feedback