Configure locale IDs
Create locale IDs and add them into the dictionary.
- Create locale IDs for English (US) and Italian languages:
- InProject view, right-clickModeland select .
- Hover-over the object, select, and enterLocaleIds.
- InProperties, at the top, selectand selectVariable.
- Double-click the variable name and enteren-US.
- SelectInt32and selectLocaleId.TIP: If you do not see the required option, select theShow allcheckbox.
- For the property value, selecten-US.
- InProperties, at the top, selectand selectVariable.
- Double-click the variable name and enterit-IT.
- SelectInt32and inData Type Editor, selectShow alland selectLocaleId.
- For the property value, selectit-IT.
- Add the Italian locale into the dictionary:
- InProperties, expandTranslations.
- Double-clickLocalizationDictionary1.
- In the middle pane, at the top, selectAdd locale.
- From the list, selectit-ITand selectAdd selected locale.
Provide Feedback