- Getting started
- Using the software
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Develop an archives manager
Use the preconfigured Zip Unzip NetLogic to create, extract, and password-protect ZIP archives.
Example application

TIP:
You can download a sample project from:
ArchivesManager.zipPrerequisites
Select
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback