ZipUnzip NetLogic
The Zip Unzip NetLogic enables you to create, extract, and password-protect ZIP archives.
IMPORTANT:
This NetLogic uses a third-party library. For more information, see NuGet Gallery | SharpZipLib.
CreateZipArchive method
CreateZipArchive
methodCompress a file or a folder into a ZIP archive.
Takes the following properties:
- Source
- A full path to the file or folder to be compressed.
- Target
- A full path to the archive to generate.
- Password
- (Optional) The phrase that password-protects the generated archive.
UnzipArchive method
UnzipArchive
methodDecompresses a ZIP archive.
Takes the following properties:
- Source
- A full path to the ZIP archive to decompress.
- Target
- A folder path where the archive contents will be extracted.
- Password
- (Optional) The phrase that may be needed to extract the archive.
Provide Feedback