Integrate the interface with the NetLogics
Integrate the NetLogics with the application interface.
- InProject view, expand .
- Configure the Insert Random Data button:
- InProject view, selectInsertButton.
- InEvents, next toMouseClick event, selectand select .
- Configure the Display Query in Label button:
- InProject view, selectRunQueryButton.
- InEvents, next toMouseClick event, selectand select .
Provide Feedback