Develop a solution for importing translations
Use OPC UA communication to import translations from another project.
Application example - client, login form
![](/content/dam/dita/en/factorytalk-optix/1-10/_images/ImportTranslations1.png/_jcr_content/renditions/original)
Application example - client, logged in Italian user
![](/content/dam/dita/en/factorytalk-optix/1-10/_images/ImportTranslations2.png/_jcr_content/renditions/original)
Application example - client, logged-in American user
![](/content/dam/dita/en/factorytalk-optix/1-10/_images/ImportTranslations3.png/_jcr_content/renditions/original)
NOTE:
Download a sample project:
ImportTranslations.zipPrerequisites
- Create a Server project. See Create a project.
- Create a Client project. See Create a project.
TIP:
The Client project imports data from the Server project.
- To develop the server project
- Arrange the interface elements.
- Save the project.
- To develop the client project
- Arrange the interface elements.
- Save the project.
Application design example
![](/content/dam/dita/en/factorytalk-optix/1-10/_images/ImportTranslationsDesign.png/_jcr_content/renditions/original)
elect
to run server and client projects using the client emulator to test your project. To run the projects on a remote client, see Add a client device.
Run
Provide Feedback