Develop a multilingual login form
Create a login form that adjusts its language to the logged in user.
Application example - user picker
![](/content/dam/dita/en/factorytalk-optix/1-10/_images/MultilingualLoginForm1.png/_jcr_content/renditions/original)
Application example - English user
![](/content/dam/dita/en/factorytalk-optix/1-10/_images/MultilingualLoginForm2.png/_jcr_content/renditions/original)
Application example - Italian user
![](/content/dam/dita/en/factorytalk-optix/1-10/_images/MultilingualLoginForm3.png/_jcr_content/renditions/original)
NOTE:
Download a sample project:
MultilingualLoginForm.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example
![](/content/dam/dita/en/factorytalk-optix/1-10/_images/MultilingualLoginFormDesign.png/_jcr_content/renditions/original)
elect
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback