Create a change user form
Add a persistent login pane to the main window.
TIP:
If you want to add a login page that disappears when you log on, see Develop a login page.
- From the toolbar, select.Template Libraries
- InLibraries, search forChange User form.
- UnderComponents, dragChange User formontoUIinProject view.
- SelectClose.
- InProject view, right-clickMainWindow (type)and select .
- InProperties, create a dynamic link betweenUsersand .For more information about dynamic links, see Create dynamic links.
Provide Feedback