InformationModel.AddTranslation(localizedText, localizationDictionary)
Adds a new key in the project
LocalizationDictionary
, which name corresponds to the value of the TextId
property of the first argument. LocaleId
and Text
properties, it also adds the translated string. The second argument is optional and indicates the LocalizationDictionary
to which the key is added.
IMPORTANT:
You must specify the second argument if the project contains more than one
LocalizationDictionary
.void AddTranslation(LocalizedTextlocalizedText, IUAVariablelocalizationDictionary);
Arguments
- localizedText(LocalizedText)
- A C# object with properties that identify the key and any translated string to add.
- localizationDictionary(IUAVariable)
- A C# object that represents aLocalizationDictionary.
Example
The following example shows an API that adds a
NewKey
key and a New translation
string for the en-US
locale.var myLocalizedText = new LocalizedText("NewKey", "New translation", "en-US"); InformationModel.AddTranslation(myLocalizedText);
Provide Feedback