Write log messages
Use C# APIs to generate log messages.
The APIs are supplied by the static
Log
C# class.
TIP:
If the log messages are generated by
FactoryTalk Optix Studio
at design time or by a FTOptixApplication
at runtime on a connected target, you can display the log messages in the FactoryTalk Optix Studio
Log
pane. You can also display the message category in the Module
column of the Log
pane.Provide Feedback