Asynchronous task
Create asynchronous tasks to run code asynchronously.
TIP:
FactoryTalk Optix Studio
provides C# class specifications that exhibit the constructors that you can use for creating asynchronous tasks. The constructors are based on the .NET Framework C# System.Threading.Tasks.Task
class, which represents an asynchronous task. See Task Class.Available classes
You can use these classes to create asynchronous tasks:
- PeriodicTask
- A task that runs code at regular time intervals.
- DelayedTask
- A task that runs code after a time delay.
- LongRunningTask
- A task that requires significant time or CPU resources.
Provide Feedback