Add NuGet packages
Some library widgets and scripts require specific NuGet packages to be installed.
IMPORTANT:
FactoryTalk Optix Studio
supports only .NET libraries with the .NET Standard 6.0 destination framework.Provide Feedback