Checkbox example

Checkbox example

Use this object to set and view a Boolean value at runtime.
Selected checkbox
The associated variable value is True.
Cleared checkbox
The associated variable value is False.
Checkbox example
animated graphic showing selecting and clearing a Checkbox

Use case

Enable or disable functions or features within a
FactoryTalk Optix Application
. For example, toggle a graph that visualizes data.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal