Configure a Dropdown button
Configure a
Dropdown button
object by linking it with a container object type.- InProject view, create a container object type.For example, create aPanel (type)
- Create aDropdown Button.
- InProperties, create a dynamic link between thePanelproperty and the container object type.For more information about dynamic links, see Create dynamic links.
Provide Feedback