- Getting started
- Using the software
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Event logger example
Use this object to record the properties of one or more selected event types that are generated by a specific node, including its child nodes, or by any node in the project, and store them in a database.
Use case
Record and display the history of events of interest, for example the activation of alarms.
Provide Feedback