Configure a Navigation panel

Configure a Navigation panel

Configure a
Navigation panel
by referencing Panel objects as tabs.
  1. In
    Project view
    , create or select a
    Navigation panel
    object.
  2. Create
    Panel
    types that you want to reference as tabs in the
    Navigation panel
    .
  3. Select
    Navigation panel
    . In
    Properties
    add tabs by selecting
    Add
    next to
    Panels
    .
  4. Create dynamic links between
    Panel
    properties and
    Panel
    types.
    For more information about dynamic links, see Create dynamic links.
  5. Expand the
    Panel#
    categories to set optional panel properties for each tab on the navigation panel:
    • Title
      . Enter the title of the tab.
    • Image path
    The image overrides the panel
    Title
    or
    BrowseName
    . For seamless integration with the UI, use correctly sized flat images with a transparent background.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal