- Getting started
- Using the software
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Option button example
Use this object to select an item from a mutually exclusive group of options at runtime.
TIP:
To create a group of mutually exclusive options, create several different
Option button
objects under a single container object. Option button example

Use case
Choose an option that excludes other options. For example, select an item from a list of alternative mechanical components.
Provide Feedback