Vertical layout example

Vertical layout example

Use this object to lay out the interface elements in the X-axis evenly.
Horizontal layout example
The positioning and distance between the buttons depend on the margins set on these buttons.

Use case

Lay out interface elements vertically. For example, lay out buttons or other objects.
TIP: To achieve a different order of the interface elements, arrange the objects in the model.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal