Open FactoryTalk Optix Studio web version
You can open
FactoryTalk Optix Studio
in a web browser. Open a clean session to remove all your projects in FactoryTalk Optix Studio web editor
that are not synchronized with GitHub®
.Prerequisites
- Sign in toFactoryTalk Hub.TIP: For more information aboutFactoryTalk Hub, see.FactoryTalk HubOnline Help
- From the available apps, selectFactoryTalk Optix.
- To openFactoryTalk Optix Studio web editor:
- SelectOpen in Browser.
- To openFactoryTalk Optix Studio web editorand remove all yourFactoryTalk Optix Studio web editorprojects that are not synchronized with GitHub:IMPORTANT: Opening a clean session permanently removes all yourFactoryTalk Optix Studio web editorprojects that are not synchronized with GitHub.
- Select the drop-down arrow afterOpen in Browserand selectOpen a clean session.
- In the dialog, selectYes.
Provide Feedback