Installation and updates
You can install
FactoryTalk Optix Studio
or access it from the supported web browser through FactoryTalk Hub
.FactoryTalk Optix Runtime
Runtime software that is deployed to
FactoryTalk Optix Application
client systems. The software required for client systems varies depending on the operating system. On Rockwell Automation, Inc.
client systems, the required software is preinstalled.FactoryTalk Optix Application Update Service
If necessary,
FactoryTalk Optix Studio
automatically updates the FactoryTalk Optix Application Update Service
when deploying an FactoryTalk Optix Application
to the client system. Once the update completes, the application deployment continues.
IMPORTANT:
On
Microsoft®
Windows®
client systems, you must upgrade the FactoryTalk Optix Application Update Service
manually by updating FactoryTalk Optix Runtime
Tools installation. See Install FactoryTalk Optix Runtime.Provide Feedback