- Getting started
- Using the software
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Activate a FactoryTalk Optix Runtime license
Use a
FactoryTalk Optix Runtime license
to run FactoryTalk Optix Applications
without any limitations on client devices.- To activate an online client device throughFactoryTalk Hub, open the license applet and log on toFactoryTalk Hub.
- To activate an online client device through a license code:
- Obtain the license code from your organization owner or organization administrator.TIP: An organization owner or organization administrator can obtain the code fromFactoryTalk Hub.
- Open the license applet and enter the license code.
- To activate an offline client device through another online device:
- Obtain the license code from your organization owner or organization administrator.TIP: An organization owner or organization administrator can obtain the code fromFactoryTalk Hub.
- On the offline client device, open the license applet and enter the license code.
- Move theActivation Requestfile from the offline device to the online device.
- On the online device, open the license applet and selectActivate Offline.
- Enter the license code.
Provide Feedback