Editor
The editor for an object is the central canvas for designing an object. Each editor for an object opens in a separate tab. Mouse over the tab to see the path of the object.
The editor toolbar for an object contains buttons that apply to the selected object. The buttons displayed depend on the object selected in the editor. In general, the buttons position the object on the canvas of the editor. For example, the buttons change the order of stacked objects and position the object on the top, bottom, or either side of the canvas. Buttons are disabled in the toolbar if an object is not selected on the editor canvas.
If you mouse over a tab to select
without saving the project, you are prompted to save your changes.

Provide Feedback