Output pane

Output pane

The
Output
pane contains columns of message information and buttons to perform tasks on the
Output
pane. By default, the
Output
pane displays errors of minimum and maximum severity and information messages. Enable
Advanced mode
to display information in the
Output
pane.
Select the arrow in the column heading to display the messages in ascending or descending order. Message columns support filtering.
Output pane columns
Column
Description
Message security level
Error
Maximum severity message
Warning
Minimum severity message
Info
Information message
Code
Message ID code. This code is for predefined messages only.
Timestamp
The time the message was logged.
Category
The category of the FactoryTalk Optix Platform message or module that generated the message.
Object
Any element referenced by the message.
Message
The content of the message.
Output pane buttons
Item
Description
Error
Display or hide error messages of maximum severity.
Warning
Display or hide error messages of minimum severity.
Info
Display or hide information messages.
Display or hide first level verbose messages for troubleshooting.
Display or hide second level verbose message for troubleshooting.
Open the output logs folder. For more information, see System log.
Delete all messages from the
Output
pane, regardless of the selected display. Messages are not deleted from log files.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal