Configure a switch to simulate alarms
Configure a switch that simulates Motor1 alarms.
- InProject view, double-clickPage2 (type).
- Right-clickPage2 (type)and select .
- InProperties, create a dynamic link betweenCheckedand theMotor1Alarmvariable.For more information about dynamic links, see Create dynamic links.
- In the editor, arrangeSwitch1according to your preferences.
Switch to simulate alarms at the bottom of Page2
![](/content/dam/dita/en/factorytalk-optix/1-10/_images/quick_start_alarm_switch.png/_jcr_content/renditions/original)
At runtime:
- Toggle the switch to trigger an alarm.
Provide Feedback