Configure an alarm event logger
Store logs about past events related to alarms in a database.
- InProject view, right-clickDataStoresand select .
- Hover-overEmbeddedDatabase1, select, and enterAlarmDB.
- From the toolbar, select.Template Libraries
- InLibraries, search forAlarms Event Logger.
- UnderComponents, dragAlarms Event LoggerontoLoggersinProject view.
- SelectClose.
- InProject view, selectAlarmsEventLogger1.
- InProperties, create a dynamic link betweenDatabaseand .For more information about dynamic links, see Create dynamic links.
Provide Feedback