Corrected anomalies in this release

The list identifies the anomalies corrected in
FactoryTalk Optix
1.1.0.
Use the identification information in parenthesis to track the anomaly in future releases or for reference when receiving assistance from Customer Support with a related issue.
Error opening project located on OneDrive [1911544]
When a project is located on OneDrive, pulling an update from the remote repository may result in an error when the project is opening. Restart
FactoryTalk Optix Studio
and reopen the project.
This anomaly first identified in version 1.0.2.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.