View alarm log events in UTC time zone
At runtime, the
Data Grid
object of the Alarm History Grid
widget displays the date and time in the Timestamp
column. The time appears in the local time zone of the device using the LocalTime
property of the events. View alarm log events in the UTC standard time zone by configuring the Time
property of events.- In the main toolbar, select.Template Libraries
- InTemplate Libraries, fromWidgets, drag theAlarm History Gridobject to the desired folder in theUIfolder.The widget appears in the node.
- With theData gridof the widget selected, in theTextproperty of theTimestampor other column, select.Change Dynamic Link
- In the Dynamic Links window, select.
- ChooseSelect.
Provide Feedback