Create an alias
Create an alias to create a variable type that points to a node with a
NodeId
property. Create the alias in either an object or a parent node.- InProject view, select the object or object type to contain the alias.
- InProperties, selectand then selectAlias.Alias#appears inPropertiesand contains theKindproperty.
- (optional) Mouse over the end of the alias name, select, and then enter a new name for the alias.
- Set the alias:
- TheIf the source node can be set at design time, select the node or drag it fromProject viewto the alias value field.Kindproperty automatically contains a value with the relative reference node.
- If the source node can be set at runtime only, or setting the source node at runtime is required, inKind, selectSet Kind, select the reference type node, and then chooseSelect.
Provide Feedback