Deploy a FactoryTalk Optix Application from a folder
To deploy a
FactoryTalk Optix Application
from a folder on a shared drive or a USB drive, move the file to the client device and run the file.Prerequisites
- To deploy aFactoryTalk Optix Applicationfrom a folder
- Move the file from the shared drive to the client device.
- RunFactoryTalk Optix Applicationon the client system:
- OnWindows®client devices, double-clickFTOptixRuntime.exe.
- On Linux client devices, in the terminal, navigate to theFTOptixRuntimefile folder and enter./FTOptixRuntime.
Provide Feedback