- Getting started
- Using the software
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Duplicate a client device
Duplicate a client device to configure another similar client device.
- From the main toolbar, next to, select the target client device drop-down menu.Run
- (optional) InClient device settings, to display only the active remote client devices, toggleActive remote devices.TIP: Refresh remote client devices by selectingRefresh.
- Select a client device.
- Select.Duplicate
Configure the duplicated client device properties.
Provide Feedback