Add an image

Add an image

Add an image to the canvas to insert an empty image and then specify the image the object is to display. You can change the image that the object displays.
  1. In
    Project view
    , right-click the object or folder to contain the image and then select
    New
    Drawings
    Image
    .
  2. Double-click the empty image that appears on the canvas.
    TIP: If you resize the image to make it larger, the message "
    Double click to select a picture"
    appears.
  3. In
    Select file
    , select the image to display and then choose
    Select
    .
    TIP: If the file does not appear in
    Select file
    , select
    Import file(s)
    and in
    Import file(s)
    , select the file to import and then choose
    Select
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.