Allow interaction with a graphic object
Enable a graphic object so that users can interact with the object at runtime. Enable a graphic object in
Properties
.- InProject viewor in the window, select the container or graphic object.
- InProperties, inEnabled, select either:
- True. The graphic object allows user interaction at runtime.
- False. The graphic object prevents user interaction at runtime.
Provide Feedback