Change the properties of a graphic object
Change the properties of a graphic object to change the name, unique properties for the graphic object, as well as its appearance and behavior at runtime.
The displayed properties for a graphic object depend on the selected graphic object. To open the graphic object to view its contents before changing properties, in
.
Properties
, select 
- In theProject viewor in the window, select the container or graphic object.
- InProperties, change the properties in these categories:
- Name. Select the existing name and enter a new name for the graphic object.
- Appearance. Change how the graphic object appears at runtime.
- Size and layout. Change the size and position of the graphic object at runtime.
- Events. Add methods for the events to perform at runtime when the user performs, or the system prompts an action.TIP:Gauge graphic objects containValueandGaugecategories. If theMinimum valueandMaximum valueproperties of a gauge change continuously and rapidly, the performance of the runtime application is impacted because the gauge must be redrawn with each change.
Provide Feedback