Copy a graphic object
Copy a graphic object to duplicate the configuration of the graphic object. Copied graphic objects create consistency and save time when creating graphic objects.
- InProject viewor in the window, select the container or graphic object.
- Right-click the graphic object and selectCopyor press .
- Right-click inProject viewor the window and selectPasteor press . The graphic element is pasted on top of the copied graphic element.
- Drag the new graphic object off the copied graphic object.
Provide Feedback