Prevent changes to a graphic object
Lock a graphic object to prevent changes to the object. Unlock an object to allowed continued changes.
- InProject viewor in the window, mouse over the container and select either:
- . The icon changes toLockand the graphic object is locked.Unlock
- . The icon changes toUnlockand the graphic object is unlocked.Lock
Provide Feedback