Specify the visibility of a graphic object
Determine whether a graphic object is visible in the window at runtime.
- In the window orProject view, select the container or graphic object.
- InProperties, inVisible, select either:
- True. The graphic object appears in the window at runtime.
- False. The graphic object does not appear in the window at runtime.
Provide Feedback