Container objects

Container objects

Container objects include:
Object
Description
Panel
Simple container for graphic objects that constitute a dialog box or widget.
By default, each new panel has a fixed width and height and is aligned with the top left corner of the parent object.
Screen
A container for graphic objects that constitute a specific interface.
By default, each new screen stretches to cover the entire parent object.
Horizontal layout
Panel that automatically arranges graphic objects horizontally next to each other.
Vertical layout
Panel that automatically arranges graphic objects vertically next to each other.
Scale layout
Container that automatically scales its children graphic objects when the container aspect ratio changes.
Panel loader
Container that uses logic to display different alternative panels at runtime.
Navigation panel
Panel that contains other panels and automatically organizes panels into tabs that you can navigate.
Dropdown button
Button that, when selected, opens and closes a pop-up window.
Scroll view
Panel that can scroll to display content larger than the panel size.
Accordion
Container that contains expandable content blocks.
Window
Root graphic container. In a Presentation Engine, you can set Window to specify the initial user interface at runtime.
TIP: The
X
,
Y
, and
Always on Top
properties apply only to the Native Presentation Engine.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.