Data controls objects
Data controls objects include:
Object | Description |
---|---|
Combo box | Drop-down to select elements from project nodes or one or more databases. |
List box | List to select element within other elements or either project nodes or databases. |
Data grid | Table that presents data from project nodes or databases. |
Trend | Trend that presents values from one or more variables that are logged or read in real time. |
XY chart | Chart that displays the value of two-dimensional variables in a graph. |
Pie chart | Chart that displays model or database data in the form of a pie chart. |
Histogram chart | Chart that displays model or database data in the form of a bar chart. |
Provide Feedback