Drawings objects
Drawings objects include:
Object | Description |
---|---|
Rectangle | A rectangle or square that can be selected at runtime and for which you can customize the appearance. Use rectangles to create buttons or group other relevant objects. |
Ellipse | An ellipse or circle that can be selected at runtime and for which you can customize the appearance. |
Image | A PNG , JPG , JPEG , BMP , or SVG image. For example, a logo. |
Multistate image | An object that can have multiple image states based on the input value. Each image state may reference a different image and may have a specific opacity. If the input value does not correspond with any image state, the default value is used (first defined state). |
Advanced SVG Image | An SVG Tiny 1.2 image, which properties of individual image parts can be changed at design time or runtime. For example, an alarm may trigger a particular part of image to become red. |
Line | A line you can draw and for which you can customize the appearance. |
Polyline | A polyline and polygon that can be selected at runtime and for which you can customize the appearance. |
Provide Feedback